STM32H745: DS and RM misalignment: doc update required
(Update: Comment moved here from STM32H745: DS and RM disagree, which to believe?)
I've also verified that these errors still exist (though table/page numbers have changed) in latest docs ("DS12923 Rev 2 March 2023" and "RM0399 Rev 4 June 2023"). These were reported 4 years ago, ST stated it would be fixed in the next revision. The next DS revision came out 3 years later and this was not fixed.
(Update: There is also a separate documentation error reported in Ethernet send complete interrupt not triggered in stm32f7 , which has similarly languished.)
Having a sluggish process is one thing - this is just dysfunctional.
Could you please follow up?