Skip to main content
Graduate
January 29, 2024
Question

STM32H745, faultily write access to external memory over debugger

  • January 29, 2024
  • 0 replies
  • 562 views

tl;dr: accessing external memory over debugger results in additional unwanted write accesses to adjacent memory locations

I have an FPGA that is accessed via FMC over a 16-bit async connection (16-bit data +15-bit address), sort of like an external SRAM. The FPGA contains a PWM module with 16-bit control registers, that are memory mapped to the STM32H745 (e.g. CTRL @ 0x60000000, TIMER_PERIOD @ 0x60000002 and so on). MPU is set to strongly ordered. I set up a svd-file and generated defines, so I can access them like normal periphery, e.g.:

FPGA->TIMER_PERIOD = 0x00FF;

This should write 0x00FF to address 0x60000002. And that works fine in code (at least with async access, synchronous does not).

But, for debugging purposes I want to access these address with the debugger over SWD (J-Link or ST-Link, doesn't matter). Reading works fine. One 16-bit access to the external memory/FPGA is generated. Writing on the other hand produces four 16-bit accesses.

So writing 0x00FF to 0x60000002 via SWD results in:

one write access to 0x60000002 with correct data, but also write accesses to 0x60000000, 0x60000004 and 0x60000006 with unwanted data.

What may be the cause here?

 

 

    This topic has been closed for replies.