Skip to main content
Explorer II
November 14, 2025
Solved

STM32H745: No device found on target on a custom board

  • November 14, 2025
  • 4 replies
  • 414 views

Hello,
I designed a custom PCB using the STM32H745IIT6 (LQFP176) and I cannot connect to the MCU using SWD with an ST-LINK V2. I always get “Error in final launch sequence / No device found on target”.

Hardware summary:

  • VDD, VDDA, VREF+ → 3.3V

  • VCAP1/2/3 → 2.2 µF

  • VDDLDO → not connected

  • BOOT0 → GND

  • NRST → 10k pull-up + 100nF

  • Board current consumption: 8.5 mA

SWD wiring:

  • SWCLK → PA14

  • SWDIO → PA13

  • NRST → NRST

  • GND → GND

  • 3.3V → board 3.3V rail (sense)

  • SWO not connected

  • 10k resistors on SWCLK/SWDIO were removed for testing.

Observations:

  • PA13 measures ~0.38–0.42 V when ST-LINK is not connected (floating)

  • ST-LINK LED stays red (never turns green)

  • CubeIDE: SWD, “Connect under reset”, 1000 kHz

  • CubeMX power mode:  PWR_DIRECT_SMPS_SUPPLY.

Question:

What could cause SWD to fail with this configuration?

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Hello @Hank_Schrader and welcome to the ST community,

    You said:


    @Hank_Schrader wrote:
    • CubeMX power mode:  PWR_DIRECT_SMPS_SUPPLY.

    But according to your schematic, SMPS is almost not connected.

    mALLEm_0-1763113779637.png

    From the RM0399 / figure 22, this is the hardware configuration for the direct SMPS:

    mALLEm_1-1763114000537.png

    The question is, how did you design your board? did you refer to any reference design? 

    NUCLEO-H755 board schematics for example?

    The following are the different HW power config listed in the reference manual. Did you refer to the documentations: reference manual, the datasheet or the AN4938 before starting your design?:

    mALLEm_2-1763114211014.png

     

    4 replies

    Super User
    November 14, 2025

    Hi,

    What could cause SWD to fail with this configuration?

    Most times hardware, power setting vs real setup; or wrong connected/bad soldering/contacts.

    So whats at Vcap ? (core voltage)

    +

    try connect with CubeProgrammer , under reset. (your V2 is genuine or a "stick" ? this might not work.)

    Super User
    November 14, 2025

    Welcome to the forum.

    Please see How to write your question to maximize your chances to find a solution for best results.

     


    @Hank_Schrader wrote:

    I cannot connect to the MCU using SWD with an ST-LINK V2. ?


    Is it a genuine SY-Link?

    See: How to recognize a genuine ST-LINK/V2 versus a cloned one.

     


    @Hank_Schrader wrote:

     I always get “Error in final launch sequence / No device found on target”.?


    Where, exactly, do you get that?

    Please show the full log, and screenshots of any pop-up messages.

    See:

    How to solve connection errors when connecting and programming the STM32 target board.

    How to solve debugger connection issues.

    Explorer II
    November 14, 2025

    Hi Andrew, thanks for your reply.

    My ST-LINK V2 is genuine.
    I still get “No device found on target”, even when using CubeProgrammer with “Connect under Reset”.

    My board uses an STM32H745BI with only a 3.3 V LDO (no SMPS).
    Some power pins like VDDLDO_x, VDDSMPS, VBAT were left unconnected, so I think this wrong power configuration might be preventing VCORE from powering up, causing the SWD error.

    VCAP pins have 2.2 µF.

    I can provide logs/screenshots if needed.

    Thanks.

    mƎALLEmAnswer
    Technical Moderator
    November 14, 2025

    Hello @Hank_Schrader and welcome to the ST community,

    You said:


    @Hank_Schrader wrote:
    • CubeMX power mode:  PWR_DIRECT_SMPS_SUPPLY.

    But according to your schematic, SMPS is almost not connected.

    mALLEm_0-1763113779637.png

    From the RM0399 / figure 22, this is the hardware configuration for the direct SMPS:

    mALLEm_1-1763114000537.png

    The question is, how did you design your board? did you refer to any reference design? 

    NUCLEO-H755 board schematics for example?

    The following are the different HW power config listed in the reference manual. Did you refer to the documentations: reference manual, the datasheet or the AN4938 before starting your design?:

    mALLEm_2-1763114211014.png

     

    Technical Moderator
    November 14, 2025

    The original question has been answered. Your issue is in your HW especially the power config. The follow-up is here