STM32H745 Not Connecting - "No STM32 Target Found" Error
I am facing an issue where my STM32H7 board is not detected using STM32CubeProgrammer. I am using an STLINK-V3SET programmer, and the following error keeps appearing:
Error log:
17:04:59 : UR connection mode is defined with the HWrst reset mode
17:04:59 : ST-LINK SN : 0028001E3233510739363634
17:04:59 : ST-LINK FW : V3J13M4B5S1
17:04:59 : Board : STLINK-V3SET
17:04:59 : Voltage : 3.29V
17:04:59 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
17:06:59 : UR connection mode is defined with the HWrst reset mode
17:06:59 : ST-LINK SN : 0028001E3233510739363634
17:06:59 : ST-LINK FW : V3J13M4B5S1
17:06:59 : Board : STLINK-V3SET
17:06:59 : Voltage : 3.29V
17:06:59 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
Setup Details
- Board: STM32H745xi series
- Debugger: STLINK-V3SET
- Software: STM32CubeProgrammer
- Voltage: 3.3V confirmed
Any help or suggestions would be greatly appreciated. Thanks in advance!