Skip to main content
Graduate
January 15, 2025
Solved

STM32H745 QSPI // SPI Mode 1 not possible?

  • January 15, 2025
  • 1 reply
  • 1097 views

Moved from the MPUs forum - H7 is an MCU


We are planning to use an STM32H745 in a high-temperature QSPI-Application with a custom QSPI device.

This custom device only supports SPI Mode 1, i.e. CPOL = 0, CPHA = 1.

From the STM32 QSPI Documentation and reference manual and as told by @TDK it looks like only Mode 0 (0/0) and Mode 3 (1/1) are possible with QSPI.

ChrisOKay_1-1736936300428.png

ChrisOKay_0-1736939189100.png

CubeMX also only offers Clockmodes "low" and "high", the corresponding tool tips are "QPSI_CLOCK_MODE0/3"

ChrisOKay_0-1736935786861.png

"Sample shifting" also only applies to incoming data according to the documentation, i.e. it will not change the CPHA.

So my question is: Is there still a (low-level/hack) way to get SPI Mode 1 working on an STM32H745?

    This topic has been closed for replies.
    Best answer by ChrisOKay

    It seems that it is not possible via a software solution. So we are taking a hardware approach by using an inverter with a low propagation delay on the clock line. This way, we should be able to turn Mode 3 into Mode 1 (at the risk of loosing a few MHz datarate due to the additional delay).

    1 reply

    ChrisOKayAuthorAnswer
    Graduate
    January 16, 2025

    It seems that it is not possible via a software solution. So we are taking a hardware approach by using an inverter with a low propagation delay on the clock line. This way, we should be able to turn Mode 3 into Mode 1 (at the risk of loosing a few MHz datarate due to the additional delay).