Skip to main content
Visitor II
May 21, 2024
Solved

STM32H745 with WIFI

  • May 21, 2024
  • 2 replies
  • 1312 views

Hello,

I plan to use STM32H745 controller with touchGFX for UI. Additionally need WIFI capability. 

What options are available if WIFI is to be used with STM32H745? 

I dont want to invest time in developing a communication protocol to communicate with a WIFI module.

Are there any ready made options available from both Hardware and Firmware side? 

Please suggest any development boards which can be used to accelerate development.

Thanks 

Anuj 

    This topic has been closed for replies.
    Best answer by STTwo-32

    Hello @ATank.1 

    If you are looking for an evaluation Board with integrated Wi-Fi Module, I suggest you use the STM32H7B3I-DK - Discovery kit with STM32H7B3LI MCU - STMicroelectronics. If you are looking for a board embedding an STM32H745 MCU, you can use the STM32H745I-DISCO - Discovery kit with STM32H745XI MCU - STMicroelectronics which embed an STMod+ extension that you can use to connect a Wi-Fi module such as the ESP-01.

    Best Regards.

    STTwo-32

    2 replies

    STTwo-32Answer
    Technical Moderator
    May 21, 2024

    Hello @ATank.1 

    If you are looking for an evaluation Board with integrated Wi-Fi Module, I suggest you use the STM32H7B3I-DK - Discovery kit with STM32H7B3LI MCU - STMicroelectronics. If you are looking for a board embedding an STM32H745 MCU, you can use the STM32H745I-DISCO - Discovery kit with STM32H745XI MCU - STMicroelectronics which embed an STMod+ extension that you can use to connect a Wi-Fi module such as the ESP-01.

    Best Regards.

    STTwo-32

    Super User
    May 21, 2024

    There are many WiFi modules available on the market, with a variety of standard interfaces - UART, SPI, etc ..

    AndrewNeil_0-1716285162741.png

     

    eg, only yesterday:

    https://community.st.com/t5/stm32-mcus-wireless/connecting-stm32f7-disco-board-to-wifi-network-using-esp8266/m-p/676684#M19151