STM32H745i Disco Deadlock when Clock Frequency is 480MHz
I tried flashing a project created for the STM32H745I-DISCO board in CubeMx. I configured clock speed for the M7 core to 480MHz and the M4 core speed to 240MHz. After flashing, if i disconnect the board, the deadlock occurs. Then i have to pull up the boot0 pin and erase full memory in-order to get out of deadlock. Even then, if i disconnect again after flashing the problem repeats.
If my clock frequency is less than 400, It is working fine. I guess it is the problem of power supply selection. Anyone has solution?
Thanks.