STM32H747-DISCO SPI problems
Using the STM32H747I-DISCO, I am having problems getting SPI working at all.
I am using SPI5, to allow connecting an X-NUCLEO-NFC08A1 directly via the Arduino headers.
I do not see any data on the SCK line and HAL_SPI_Transmit() always fails.
Looking in stm32h7xx_hal_spi.c, I see that SPI_FLAG_EOT is never detected and so HAL_SPI_Transmit() times out with HAL_SPI_ERROR_FLAG set.
Is there a working sample showing SPI configuration and use on the STM32H747?
Can anyone suggest what I'm doing wrong?
Thanks.
Pin/port definitions:
#define SPIx SPI5
#define SPIx_IRQn SPI5_IRQn
#define SPIx_SCK_GPIO_CLK_ENABLE() __HAL_RCC_GPIOK_CLK_ENABLE()
#define SPIx_MISO_GPIO_CLK_ENABLE() __HAL_RCC_GPIOJ_CLK_ENABLE()
#define SPIx_MOSI_GPIO_CLK_ENABLE() __HAL_RCC_GPIOJ_CLK_ENABLE()
#define SPIx_CLK_ENABLE() __HAL_RCC_SPI5_CLK_ENABLE()
#define SPIx_SCK_PIN 0
#define SPIx_SCK_GPIO_PORT GPIOK
#define SPIx_SCK_AF GPIO_AF5_SPI5
#define SPIx_MISO_PIN 10
#define SPIx_MISO_GPIO_PORT GPIOJ
#define SPIx_MISO_AF GPIO_AF5_SPI5
#define SPIx_MOSI_PIN 11
#define SPIx_MOSI_GPIO_PORT GPIOJ
#define SPIx_MOSI_AF GPIO_AF5_SPI5
#define SPIx_FORCE_RESET() __HAL_RCC_SPI5_FORCE_RESET()
#define SPIx_RELEASE_RESET() __HAL_RCC_SPI5_RELEASE_RESET()Hardware setup:
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi) {
GPIO_InitTypeDef GPIO_InitStruct;
if (hspi->Instance == SPIx) {
SPIx_SCK_GPIO_CLK_ENABLE();
SPIx_MISO_GPIO_CLK_ENABLE();
SPIx_MOSI_GPIO_CLK_ENABLE();
SPIx_CLK_ENABLE();
/* SPI SCK GPIO pin configuration */
GPIO_InitStruct.Pin = SPIx_SCK_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = SPIx_SCK_AF;
HAL_GPIO_Init(SPIx_SCK_GPIO_PORT, &GPIO_InitStruct);
/* SPI MISO GPIO pin configuration */
GPIO_InitStruct.Pin = SPIx_MISO_PIN;
GPIO_InitStruct.Alternate = SPIx_MISO_AF;
HAL_GPIO_Init(SPIx_MISO_GPIO_PORT, &GPIO_InitStruct);
/* SPI MOSI GPIO pin configuration */
GPIO_InitStruct.Pin = SPIx_MOSI_PIN;
GPIO_InitStruct.Alternate = SPIx_MOSI_AF;
HAL_GPIO_Init(SPIx_MOSI_GPIO_PORT, &GPIO_InitStruct);
}
}SPI initialisation:
hspi5.Instance = SPIx;
hspi5.Init.Mode = SPI_MODE_MASTER;
hspi5.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;
hspi5.Init.Direction = SPI_DIRECTION_2LINES;
hspi5.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi5.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi5.Init.DataSize = SPI_DATASIZE_8BIT;
hspi5.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi5.Init.TIMode = SPI_TIMODE_DISABLE;
hspi5.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi5.Init.CRCPolynomial = 7;
hspi5.Init.CRCLength = SPI_CRC_LENGTH_8BIT;
hspi5.Init.NSS = SPI_NSS_SOFT;
hspi5.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
hspi5.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE; /* Recommended setting to avoid glitches */
if(HAL_SPI_Init(&hspi5) != HAL_OK) {
Error_Handler();
}