Question
STM32H747: Reducing standby mode current consumption
Hello,
We are using the STM32H747AI on a custom board and attempting to enter standby mode for power savings. The system supply is configured as "SMPS supplies LDO (no external supply)" to be able to use the boosted performance at 480MHz, but the chip still draws around 20 mA in standby mode with the M4 core disabled.
To verify these results, we performed the same measurements on the STM32H747I-DISCO board, modifying the jumpers to match the same supply configuration. The results were similar.
Is there anything specific we must do to further reduce current consumption?