STM32H747i-disco 10Mhz Uart Rx interrupt problem
Hello ST experts, i need help about using STM32H747i-disco
I'm testing Uart Tx(DMA)-Rx(Interrupt). My goal is 10Mhz uart tx-rx.
The problem is that i success 750khz, but fail to Rx when baudrate 1Mhz~10Mhz.
I set the disco 480Mhz setting (hw SB setting done for SMPS -> LDO).
Uart8 peripheral clock is 120Mhz(Max). Uart8 Oversampling changed 16 -> 8 sample.
So i can set uart8 baudrate up to 15Mbps.
I connect STM32H747i-disco CN6-D0(PJ9 uart8-rx) to CN6-D1(PJ8 uart8-tx).
So if i run uart8_tx -> uart8_rx will catch.
I have testing uart gpio speed low to very high but it is not work for my case.
Success at 750khz. Fail at >1Mhz.
Need some advise.
Thank you.