STM32H747I-Disco error: "Break at address "0x800c44e" with no debug information available, or ou..."
Getting this error and have no idea how to troubleshoot it further:
Break at address "0x800c44e" with no debug information available, or outside of program code.
<signal handler called>() at 0xfffffff1
Break at address "0x8004bf4" with no debug information available, or outside of program code.
Break at address "0x800c510" with no debug information available, or outside of program code.
The error is triggered when I try and run audio to the DMA, specifically the call to 'HAL_SAI_Transmit_DMA' inside BSP_AUDIO_OUT_Play. I'm using very similar code to the BSP audio demo, which works fine if I run it, but when I try and run it on my code base it fails.
It doesn't seem to be triggered at a consistent point in the code, just some point after I first start the DMA process.
How do I figure this one out?
Thanks!
Chris