STM32H747IX SystemClock_Config problem
I have configured the M7 clock to 480 MHz and the M4 clock to 240 MHz using the HSI as input. In SystemClock_Config routine the statement
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
is crashing the STLINK-V3 with the error message
Error in executing 'step' command ...
Target is not responding, retrying...
I had a breakpoint at that line and activated it with the Step Into (F5).