STM32H747XI EXTI interrupts of M4
Hi,
I am migrating my project from STM32F778AI to STM32H747XI and I have some issues regrading EXTI interrupt on M4 core.
I use custom board with J-link programmer.
I have simple button with hardware pull-up and I configured pin to be EXTI11 on M4 (enabling interrupts- falling edge) and it is not working. But, if I configure this pin to M7 it works perfectly..
Is there anything special that I need to do to make it work?
I read that EXTI works on M4 the same as in M7.
Thanks,
David