STM32H750 About Dual-Flash mode program in QSPI
Hello,
I may have a misunderstanding about Dual-Flash programming, so my question might seem strange.
In Dual-Flash mode, does the write speed double?
If so, I think the following code cannot achieve double the write speed in Dual-Flash mode. (stm32h7xx_hal_qspi.c)
What are your thoughts on this?
/**
* @brief Transmit an amount of data in blocking mode.
* hqspi QSPI handle
* pData pointer to data buffer
* Timeout Timeout duration
* @note This function is used only in Indirect Write Mode
* @retval HAL status
*/
HAL_StatusTypeDef HAL_QSPI_Transmit(QSPI_HandleTypeDef *hqspi, uint8_t *pData, uint32_t Timeout)
{
HAL_StatusTypeDef status = HAL_OK;
uint32_t tickstart = HAL_GetTick();
__IO uint32_t *data_reg = &hqspi->Instance->DR;
/* Process locked */
__HAL_LOCK(hqspi);
if(hqspi->State == HAL_QSPI_STATE_READY)
{
hqspi->ErrorCode = HAL_QSPI_ERROR_NONE;
if(pData != NULL )
{
/* Update state */
hqspi->State = HAL_QSPI_STATE_BUSY_INDIRECT_TX;
/* Configure counters and size of the handle */
hqspi->TxXferCount = READ_REG(hqspi->Instance->DLR) + 1U;
hqspi->TxXferSize = READ_REG(hqspi->Instance->DLR) + 1U;
hqspi->pTxBuffPtr = pData;
/* Configure QSPI: CCR register with functional as indirect write */
MODIFY_REG(hqspi->Instance->CCR, QUADSPI_CCR_FMODE, QSPI_FUNCTIONAL_MODE_INDIRECT_WRITE);
while(hqspi->TxXferCount > 0U)
{
/* Wait until FT flag is set to send data */
status = QSPI_WaitFlagStateUntilTimeout(hqspi, QSPI_FLAG_FT, SET, tickstart, Timeout);
if (status != HAL_OK)
{
break;
}
*((__IO uint8_t *)data_reg) = *hqspi->pTxBuffPtr;
hqspi->pTxBuffPtr++;
hqspi->TxXferCount--;
}
if (status == HAL_OK)
{
/* Wait until TC flag is set to go back in idle state */
status = QSPI_WaitFlagStateUntilTimeout(hqspi, QSPI_FLAG_TC, SET, tickstart, Timeout);
if (status == HAL_OK)
{
/* Clear Transfer Complete bit */
__HAL_QSPI_CLEAR_FLAG(hqspi, QSPI_FLAG_TC);
}
}
/* Update QSPI state */
hqspi->State = HAL_QSPI_STATE_READY;
}
else
{
hqspi->ErrorCode |= HAL_QSPI_ERROR_INVALID_PARAM;
status = HAL_ERROR;
}
}
else
{
status = HAL_BUSY;
}
/* Process unlocked */
__HAL_UNLOCK(hqspi);
return status;
}