STM32H750XBHX - CANFD Callback problem
Hey, I have a problem with the callback for FDCAN1. I am sending frames through ucandevices converter but the callback for FIFO0 is not called. The frames are definitely arriving, I added a test FreeRTOS and a task to receive and send frames to CAN1 and it worked very well, frames were received and sent back to the bus.
I have NVIC interrupts set up, I fiddled with the clock for CANFD and speeds, also with no effect.
Is anyone able to help me?
I am sending my project as an attachment