Skip to main content
Visitor II
May 9, 2024
Question

STM32H753 SPI data rate

  • May 9, 2024
  • 1 reply
  • 1723 views

Hello. Is the STM32H753 able to directly interface with a slave on the SPI bus, which continuously produces data at a rate of 40 Mbps for several hours? What would be the current consumption rate for such a case?

Thank you

    This topic has been closed for replies.

    1 reply

    Super User
    May 9, 2024

    Hi,

    the 40M speed is no problem, see ds :

    AScha3_0-1715283106789.png

    100M max , slave or master.

     

    > What would be the current consumption rate for such a case?

    Same as if not use SPI , almost. You can check it in Cube -> Tools ...power consumption.

     

    which continuously produces data at a rate of 40 Mbps for several hours?

    So this might be a problem : what you wanna do with these 50 GB on a cpu with 1MB RAM ??

    Graduate II
    May 9, 2024

    @AScha.3 wrote:

    ...

    which continuously produces data at a rate of 40 Mbps for several hours?

    So this might be a problem : what you wanna do with these 50 GB on a cpu with 1MB RAM ??


    Double-buffer /dev/null.  (Those who know, know.)  ;)