Question
STM32H755 : Can both M7 and M4 access both internal flash banks in parallel?
Can M4 write to part of Bank 1 when M7 code is running from Bank 1? Idea is to define a
partition at the end of Bank 1 and M4 write to it while M7 reads from it. I know this
needs some tweaking of the dts to assign both Bank 1 and Bank 2 to M4 as below. IOW, as per SoC
design, can M7 code runs from a partition on Bank 1, and read data from another partition
(128 KiB) at the end of Bank1 which is also written by M4. In DTS, I plan to update DTS
to have flash0 assigned to M4 and it has a size of 2048 KiB with partitions like below. The fundamental question is is there is bus contention possible? Assume at driver level (in Bare-Metal using HAL driver and Zephyr), any common register write are guarded through semaphore.
&flash0 {
compatible = "st,stm32-nv-flash", "soc-nv-flash";
reg = <0x08000000 DT_SIZE_K(2048)>;
partitions {
compatible = "fixed-partitions";
#address-cells = <0x1>;
#size-cells = <0x1>;
/* 768KiB RT image */
image1_partition: partition@0 {
reg = <0x0 0xc0000>;
read-only;
};
/* 128KiB settings */
configuration_partition: partition@c0000 {
reg = <0xc0000 0x20000>;
};
/* 896 KiB Archon image */
image2_partition: partition@100000 {
reg = <0x100000 0xc0000>;
read-only;
};
/* 128KiB bootloader image */
bootloader_partition: partition@1c0000 {
reg = <0x1c0000 0x20000>;
};
};
};