STM32H755Zi-Q~How to share data between cores
Currently I am just trying to share some data between cores, and right now I'm just trying to send a constant value to confirm operation.
I have this code located in a file called share.h,
typedef struct {
// shared data goes here
int16_t data;
}shared_data_t;and then I have
volatile shared_data_t * const shared_data = (shared_data_t *)0x30040000;saved in each core's main.c file.
The location is SRAM3 and according to the RM this is an optimal place to share values. It updates properly in M7, but when I check the struct in M4 it's not the same value. When googling, this was the number 1 answer, the second was the linker. I don't know where to begin with the linker, so if that is the option is there any good guides? Thank you for reading this