Skip to main content
Visitor II
February 7, 2025
Question

STM32H7A3ZIT6: undershoot and overshoot in the input pin

  • February 7, 2025
  • 3 replies
  • 632 views

Thank you so much for your continued support.

There is undershoot and overshoot in the waveform of the input pin on the STM32H7A3ZIT6. What is the acceptable duration (in nanoseconds) for it to be within specification?

Please also check the attached file.

Ryuichi_0-1738906914073.png

Sorry to trouble you, but please provide your response.

Best Regards。

 

    This topic has been closed for replies.

    3 replies

    ST Employee
    February 20, 2025

    Hello @Ryuichi

    If the IO pin is configured as an input and it is a 5V-tolerant pin, there is no issue with undershoot or overshoot as long as the voltage does not exceed VDD + 3.6V, with a maximum limit of 5.5V. Given that VDD = 3.3V, this is within acceptable limits. For more details, please refer to the datasheet, table 22 "General operating conditions". 

    Super User
    February 20, 2025

    Hi,

    first question is: what is shown on the DSO ? real overshoot or measuring artifact ?

    So can you show a pic from your measurement setup ? Just , when you make the capture, board , probe and cabels, connections, as they are.

    And also : capture a square wave output from an i/o pin of the cpu, pin setting at highest speed, to compare.

    RyuichiAuthor
    Visitor II
    March 6, 2025

    Hello Sarra.S san

    Thank you for your response.

    I have confirmed regarding the overshoot.

    I have an additional question.

    The measured undershoot is -0.5V, which is out of specification.

    This is the same question as for the overshoot, but what is the allowable duration (in nanoseconds) for it to remain within the specification range?

    Please also check the attached file.

    Ryuichi_0-1741239284580.png

    Sorry to trouble you, but please provide your response.

    Best Regards。