STM32H7S7L8H6H Unable to use Ethernet (RMII) and SDMMC2 at the same time?
Hello,
i try to configure a STM32H7S7L8H6H in CubeMX and it seems that, when Ethernet RMII is configured, SDMMC2 is unusable because there are some pins like PC1 which can't be remapped. Can this be true?
This chip is designed for external memories and i want to use microSD and eMMC.
What is the STM32H7S7L8H6HU chip? Is it a improved stepping?