STM32L0 cannot change PWR_CR_ VOS
Hi, I'm stuck on a problem with setting PWR_CR_VOS on NUCLEO-32 STM32L031K6
- I want to select HSI16-PLL as clock source
- VDD is 3.3V
- FLASH latency is set to 1WS
But I can only set PWR_CR_VOS to RANGE 2 and RANGE 3.
RANGE 1 cannot be selected, so I can't set HSI-PLL to 32MHz
where am I going wrong?
Example code:
// Set the Flash ACR to use 1 wait-state
// and enable the prefetch buffer and pre-read.
FLASH->ACR |= (FLASH_ACR_LATENCY | FLASH_ACR_PRFTEN | FLASH_ACR_PRE_READ);
//----------------------------------------------------
// 1. POWER ENABLE CLOCK and VOLTAGE REGULATOR
//----------------------------------------------------
// APB2ENR->SYSCFGEN
RCC->APB2ENR |= RCC_APB2ENR_SYSCFGEN;
// APB1ENR->PWREN: Power interface clock enable bit for PWR
RCC->APB1ENR |= RCC_APB1ENR_PWREN;
// PWR: VOS[11:2] bits (Voltage scaling range selection)
// !!! 0x0UL: FORBIDDEN
// 0x1UL: 0b01 RANGE 1 1.8V 32MHz
// 0x2UL: 0b10 RANGE 2 1.5V 16MHz
// 0x3UL: 0b11 RANGE 3 1.2V 4.2MHz
// Clear VOS bits
PWR->CR &= ~PWR_CR_VOS;
// SET RANGE 1
PWR->CR |= (0x1UL << 11U);
// Wait until ready
while (PWR->CSR & PWR_CSR_VOSF);
The value in the register is still 0x2UL, when trying to change to 0x1UL the register is 0x3UL
Where am I making a mistake that RANGE1 cannot be set to 0x1UL?