STM32L010R8 Interrupt Vector Mapping from Boot Area to App area
We need support with the interrupt vector mapping for the STM32L010R8 SoC, specifically from the Boot area to the Application area (Flash/SRAM).
We are currently developing a custom boot loader for the STM32L010R8 series and are not using the ROM-based boot loader. The issue we are encountering occurs when we jump from the Boot area (0x08000000 - 0x08001FFF) to the Application area (0x08002000). The interrupt vector table is not mapping correctly into the application flash area.
We have tried two approaches: one is direct mapping to the Flash area, and the other is mapping to a specific RAM area. According to the .map file, the mapping appears correct, but during execution, the interrupts are not being triggered, and the code is not running as expected.
Could you please provide support for this vector mapping issue? If you have any sample projects or code snippets available, please share them with us. Alternatively, if possible, could you forward this issue to the relevant application engineer for further assistance?