STM32L011 temperature sensor accuracy
I used the example code in RM, and room temperature is arround 31℃,the ADC value is 10644, calculated temperaure is 4127, does it means 41.27℃?what will happen if minus temperature?
/* Temperature sensor calibration value address */
#define TEMP130_CAL_ADDR ((uint16_t*) ((uint32_t) 0x1FF8007E))
#define TEMP30_CAL_ADDR ((uint16_t*) ((uint32_t) 0x1FF8007A))
#define VDD_CALIB ((uint16_t) (300))
#define VDD_APPLI ((uint16_t) (330))
int32_t ComputeTemperature(int32_t measure)
{
int32_t temperature;
temperature = ((measure * VDD_APPLI / VDD_CALIB) - (int32_t) *TEMP30_CAL_ADDR ) ;
temperature = temperature * (int32_t)(130 - 30);
temperature = temperature / (int32_t)(*TEMP130_CAL_ADDR - *TEMP30_CAL_ADDR);
temperature = temperature + 30;
return(temperature);
}