STM32L073 operating on low power
Hi, I am working on a project where I have a custom board with STM32L073 MCU and I want to read a color sensor (AS7341) via I2C. This will be a low power application. I will harvest energy via NFC from a smartphone (I am using NTAG I2C plus). I can get a voltage is about 2.8 V and current about 10-14 mA from the harvested energy. This will power up the color sensor and the MCU. I have been trying to operate the MCU at low power but I am unable to do it. I have tried regulating down voltage from a 3.7V 1000 mAh lipo battery to 1.8V and trying to run the MCU to get the color sensor data but I cannot do it. I tried using a logic analyzer to observe the I2C signals. For greater than 3.3V, it works fine, I am able to see the data in uart as well as in the logic analyzer but when it goes below 3.3V it doesn't work. I also tried regulating down to 2.8V from a battery, still doesn't work. I think I am missing something on how to operate the STM32 MCU in low power mode. Please let me know what I need to change in my code or board design. I have attached both below. (The circuit diagram is only for the STM32 MCU board. I am using a breakout board for the AS7341 to connect it to the MCU).
I am not much familiar with using low power modes, so I know I might need to make some changes in the clock configuration or something in the code or hardware side, but I am not sure what to do. Any help would be appreciated.