STM32L152RE 5V tolerant pin and ADC
Hello,
I have a STM32L152RE and I use PA1 (Pin type is FT 5v tolerant) as ADC_IN1. Vdd is 3.3V and the voltage on PA1 usually is around 5V and sometimes it drops to 2.5V ( when I need to take the measure).
Several comments on various blog said that usually is not possible have voltages above 4V even if the pin is FT if the pin is used as ADC. I searched everywhere in the datasheet and there is any note for the STM32L152RE. So I'd like to know if I can apply safely 5V on that pin.
Regards,
Riccardo