STM32L431 I2C master transmitter freezes if SCL is pulled down externally when it starts
When I2C master transaction (both Rx and Tx) is started while SCL is pulled to 0 externally, it goes into BUSY mode (I2C_ISR=0x8001) and remains there indefinitely, without setting any interrupt-generating flag, even after the external SCL->0 is removed.
This is extremely simple to reproduce, well, just short SCL to ground and write any START-containing "command" to I2C_CR2; and then remove the short, while observing I2C_ISR. It's enough to do it in debugger with stopped processor, the result is obvious enough.
I expected, that either
1. I2C throws a BERR (I would prefer this, but BERR's description says its scope is limited to a very particular bus error involving only STOP and START - and the BERR-related erratum dismisses its real-world usability entirely), or,
2. upon removal of SCL->0 I2C proceeds with the transaction as normally.
Documentation says, it's 2.:

This issue - which I consider to be a flaw - makes implementation of a sturdy I2C master based entirely on I2C interrupts impossible; there must be an additional timeout implemented. Together with TXIS-when-NACK issue, it makes proper I2C software significantly more complex than if the I2C would be correctly implemented according to documentation.
JW