STM32L431KC hangs on reset
I am working on a custom board and I have noticed that whenever the device resets, it becomes unresponsive.
The reset causes that hang the microcontroller:
- Calling NVIC_SystemReset from firmware
- Having firmware stuck and receiving a signal from IWDG
- Manually grounding the NRST pin.
The debugger shows that the program starts running in a lop at addresses 0x1FFF2XXX, which would be a RAM stack, I suppose?..
My FW memory map looks like this:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 16K
BOOT (rx) : ORIGIN = 0x08000000, LENGTH = __boot_size
FLASH (rx) : ORIGIN = 0x08000000+LENGTH(BOOT), LENGTH = __program_size
FLASH2 (rx) : ORIGIN = ORIGIN(FLASH)+LENGTH(FLASH), LENGTH = __program_size
DATA (rx) : ORIGIN = ORIGIN(FLASH2)+LENGTH(FLASH2), LENGTH = __data_size
}My USER_VECT_TAB_ADDRESS is defined and VECT_TAB_OFFSET is non-zero due to isr_vector not being at the beginning of the FLASH region.
So far I tried downloading a dummy firmware with only USART and IWDG enabled, with no custom remapping of memory - the issue persists. At the moment I cannot ground the NRST pin directly to see what happens, but grounding the external jumper input that is supposedly directly connected to the NRST pin also renders the firmware unresponsive.
Is there anything in particular I can do to pinpoint the problem? I don't currently have the electric scheme of the board to check how NRST is connected, but I wondered if I can do some more testing to see if the firmware could be at fault.