STM32L476 Changing VRef for ADC precision
Hi I want to sample low voltage signals with STM32L476 so I figured it would be a good option to reduce reference voltage and I found this part in the MCU datasheet:

Now I am using ADC in dual mode and sampling 8 bit so it is not too precise for low voltages.
In ADC1 settings, there is a checkbox:

Is it enough to set it to shift Vref from 3.3 to 2.048 or how should I set my reference voltage to 2.048?
Also If I decide to use an external Vref can I just connect lets say 1V to Vref+ for MCU to change Vref for ADC to 1V from 3.3V.