STM32L4A6 and dual Bank (BFB2)
Hello,
I'm having an issue with the STM32L4A6(1Mb) and the dual-bank.
First of all, I tried with the NUCLEO-L476 and a simple blink led. It worked fine.
Now, my project is based on a STM32L4A6, but the firmware doesn't start in BANK2.
For simplicity, I did the same program blink led as for the STM32L476
This is what I implemented in SystemInit():
VECT_TAB_OFFSET is 0x80000
void SystemInit(void)
{
#if defined(USER_VECT_TAB_ADDRESS)
/* Configure the Vector Table location -------------------------------------*/
FLASH_OBProgramInitTypeDef FLASH_OBProgramInit = {0};
//Read all options bits
HAL_FLASHEx_OBGetConfig(&FLASH_OBProgramInit);
//Check the BFB2 bit
if (FLASH_OBProgramInit.USERConfig & FLASH_OPTR_BFB2)
SCB->VTOR = VECT_TAB_BASE_ADDRESS | VECT_TAB_OFFSET;
else
SCB->VTOR = VECT_TAB_BASE_ADDRESS;
#endif
/* FPU settings ------------------------------------------------------------*/
#if (__FPU_PRESENT == 1) && (__FPU_USED == 1)
SCB->CPACR |= ((3UL << 20U)|(3UL << 22U)); /* set CP10 and CP11 Full Access */
#endif
}
I flashed the same code at 0x8000000 and at 0x8080000(half memory).
I did the workaround as mentionned in the errata sheet:

But nothing to do, the program never starts in BANK2.
May be an idea?
Pierre