Skip to main content
Explorer
November 25, 2025
Question

STM32L4R5ZIT6P ESD Damage

  • November 25, 2025
  • 3 replies
  • 169 views

Hello, 

 

I may have accidently either shorted or applied voltage to my UART TX and RX pins on my MCU which is on a custom PCB and now my PCB is pulling +60 mA of current under load. I am now experiencing difficulty programming the chip and I am getting errors such as "unable to recognize device" and "check power and cable". I wonder if exposing my UART pins to ground or power caused some sort of ESD or electrical damage inside the MCU and that combined with a longer power supply cable is causing a jump in current that makes it difficult to flash now?

 

Thank you.

    This topic has been closed for replies.

    3 replies

    Super User
    November 25, 2025

    Shorting GPIO pins to GND or VDD is not ESD damage and generally will not damage the chip.

    > PCB is pulling +60 mA of current under load

    So there likely is hardware damage. Could be that there are hardware issues that have caused damage cumulatively. Could be pins seeing overvoltage.

    Technical Moderator
    November 25, 2025

    Dear @ym21 ,

    Indeed it seems more like an EOS - Electrical Over Stress beyond the pins and product AMR - Absolute Maximum Rating . Can you keep your Reset/pin low and measure the current under reset and let us know ? If the current is excessive not few mA , the Device is damaged for sure .

    Hope it helps you ,

    STOne-32

    ym21Author
    Explorer
    November 25, 2025

    When I pull NRST down to ground, the PCB is pulling elevated levels of current.