STM32L562 max pin voltage / pins driven in unpowered state / current injection on pins
Hello ST,
1. ds12736 Rev.4 states in Table 24 that the abs. max. voltage on any pin is at least +4.0V (but this may be further limited by an injection current limitation)
2. ds12736 Rev.4 states in Note 4 on p.145: "Positive injection (when VIN > VDDIOx) is not possible on these I/Os and does not occur for input voltages lower than the specified maximum value."
3. ds12736 Rev.4 states in Table 25 that I_inj(pin) is specified as -5/+0 mA on all pins.
4. AN4899 Rev.3 says on p.13: "Positive-injection current is the current induced when VIN > VDD." and "0 mA means that current injection can damage the GPIO and induce STM32 malfunction."
These statements taken together seem to be contradictory.
So the question: May STM32L562 GPIO pins be driven in a range from 0 V to 3.3V when VDD and/or VDDIO is unpowered or below 3.3V? The datasheet seems to imply "Yes", but AN4899 seems to indicate the opposite in the context of the specified I_inj(pin).