STM32L562RET6 Current Consumption Reduction in low power run mode.
I have been trying to reduce current consumption in a custom board and have seen that current is not getting below 9mA for microcontroller , i am running system on MSI at 2MHz and ABP and AHB peripherals both are at 2MHz ,and to enter in low power run mode i use HAL_PWREx_EnableLowPowerRunMode(), but no effect same current at 2MHz and at 48MHz about 6mA ,can it reduced to 1mA or even in microAmperes