Skip to main content
Explorer
December 2, 2025
Question

STM32N6 DCMIPP Horizontal Distortion Beyond Certain Line Length

  • December 2, 2025
  • 0 replies
  • 88 views

Hey all,

I have a Sony IMX686 camera module connected to the STM32N6 Discovery Kit, streaming video to the on-board LCD. The sensor outputs a single-stream RAW Bayer format on Virtual Channel 0, and the DCMIPP receives the data correctly — up to a certain horizontal resolution. The issue appears to be related to a bytes-per-line limit within the DCMIPP or its DMA pipeline.

When the IMX686 outputs RAW8, the DCMIPP can only handle horizontal line lengths up to 1552 pixels. If I increase the width beyond 1552 px (e.g., to 1668 px), I begin to see horizontal distortions in the lower portion of the frame. These distortions worsen as the width increases. See the images below.

bwelte1_0-1764644769466.pngbwelte1_1-1764645262542.jpeg

As the width increases further, the distortion grows and eventually affects most of the frame (shown below).

bwelte1_3-1764645353470.png

When switching the sensor to RAW10, the exact same distortion appears, but it goes away when I reduce the horizontal resolution to 1232 pixels. This matches the expected scaling:  
1552 * 8 / 10 ≈ 1241 → nearest practical width/alignment is 1232
This makes it look like the system is hitting a maximum bytes-per-line limit that is the same for RAW8 and RAW10.

Additional Notes:

  • Changing the sensor data rate or PHYBitrate does not affect the distortion.

  • The number of bytes the sensor outputs per line is fixed; only the active pixel count changes due to digital cropping. The pixels which are cropped out are still sent over but removed during stats removal.

  • I verified this by disabling:

    • Decimation

    • Bad pixel removal
      These ISP features do not affect the distortion pattern.

  • This suggests the corruption (if introduced inside the DCMIPP pipeline), is likely in one of the circled ISP stages shown below .

bwelte1_5-1764645696861.png

This behavior strongly suggests a DCMIPP line-buffer or DMA stride/byte-limit issue, where the hardware can accept only around ~1550 bytes per line before corruption begins. The progressive distortion (starting at the bottom and moving upward as width increases) also resembles a buffer overflow or line-stride misalignment.

Any insight on what might be causing this, is there such a line length limit? What buffer might be overflowing here if this is the case?

Thanks :)

 

    This topic has been closed for replies.