STM32N6 HPDMA not copying data
Hello,
another day, another N6 "issue" :)
I want to do RAM to RAM copy by HPDMA, but the data never get copied from Src to Dest, Dest always stays unmodified. I have checked the 'DMA_RAMToRAM' example for N6 and went from there, but with no success.
DMA Init:
__HAL_RCC_HPDMA1_CLK_ENABLE();
HAL_NVIC_SetPriority(HPDMA1_Channel1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(HPDMA1_Channel1_IRQn);
handle_HPDMA1.Instance = HPDMA1_Channel1;
handle_HPDMA1.Init.Request = DMA_REQUEST_SW;
handle_HPDMA1.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
handle_HPDMA1.Init.Direction = DMA_MEMORY_TO_MEMORY;
handle_HPDMA1.Init.SrcInc = DMA_SINC_INCREMENTED;
handle_HPDMA1.Init.DestInc = DMA_DINC_INCREMENTED;
handle_HPDMA1.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_HALFWORD;
handle_HPDMA1.Init.DestDataWidth = DMA_DEST_DATAWIDTH_HALFWORD;
handle_HPDMA1.Init.Priority = DMA_LOW_PRIORITY_HIGH_WEIGHT;
handle_HPDMA1.Init.SrcBurstLength = 2;
handle_HPDMA1.Init.DestBurstLength = 2;
handle_HPDMA1.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0 | DMA_DEST_ALLOCATED_PORT0;
handle_HPDMA1.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
handle_HPDMA1.Init.Mode = DMA_NORMAL;
if (HAL_DMA_Init(&handle_HPDMA1) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMA_ConfigChannelAttributes(&handle_HPDMA1,
DMA_CHANNEL_PRIV | DMA_CHANNEL_SEC | DMA_CHANNEL_SRC_SEC | DMA_CHANNEL_DEST_SEC) != HAL_OK)
{
Error_Handler();
}And code:
__attribute((aligned(32))) uint16_t _dataSrc[128];
__attribute((aligned(32))) uint16_t _dataDst[128];
...
if (HAL_DMA_Start_IT(&handle_HPDMA1, (uint32_t)&_dataSrc[0], (uint32_t)&_dataDst[0], 256) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMA_PollForTransfer(&handle_HPDMA1, HAL_DMA_FULL_TRANSFER, 10) != HAL_OK)
{
Error_Handler();
}_dataSrc and _dataDst are global variables at 0x3400xxxx region (FLEXRAM).
_dataSrc contains data, checked.
When I use memcpy, that works. When I use GPDMA1 with exactly the same parameters, that also works. But HPDMA doesn't. No error I can see happened, not stuck in Error_Handler, no HardFault.. The code just executes normally and continues after that, so the transfer completed correctly. Yet the _dataDst stays unmodified.
L1 D-cache was off for these tests.
What am I missing?
Thank you.