Skip to main content
Visitor II
June 26, 2025
Question

STM32N6 in Nucleo XIP mode

  • June 26, 2025
  • 1 reply
  • 392 views

I have successfully completed using STM32N6 in LRUN mode and got the proper result and now I want to use Execute in place mode so please provide with all its related documents and videos.
When I try to run appli code in DEV mode it does not run, it displays "Target is not responding, retrying..." and also when i try to use xspi clock to 200MHz and main clock to 800MHz even FSBL shows the same error.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    June 27, 2025

    Hello @1anku and welcome to the community;

     

    Are you able to flash/run the official example Template_FSBL_XIP ?

    This project is targeted to run on STM32N657X0H3QU device on NUCLEO-N657X0-Q board.

    I recommend you to look to the readme file for information on how to use the Template FSBL XIP.

    Thank you.

    Kaouthar