STM32N6 minimal hardware design
Hi there,
I'm designing a custom PCB using the STM32N657Z0 MCU. The design is extremely space-constrained, so I try to leave out everything I can. Since this deviates quite a bit from the reference design (well, the N6 Discovery kit, that is) I'd love to get some clarifications from someone from ST experienced with the N6 hardware side of things:
1. I'm not using USB at all. What should I do with the USB power pins VDD33USB and VDDA18USB, can I just connect them to ground? Or leave unconnected? Are the tuning resistors OTG1_TXRTUNE and OTG2_TXRTUNE necessary when I don't use USB, or can I just leave these pins unconnected? I assume all other USB pins (data etc) can just be left floating.
2. I do not use any external crystals or oscillators, can I just leave the OSC_OUT, OSC_IN, OSC32_OUT and OSC32_IN pins unconnected?
3. I use an external regulator to supply the VDDCORE domain (instead of the internal SMPS). Am I understanding AN5967 and AN6000 correctly that in this case the pins for the internal SMPS (VDDSMPS, VDDA18PMU, VFBSMPS, VLXSMPS) must all be connected to ground?
4. Since the external switching regulator supplying VDDCORE (see last question) is pretty delicate I try to copy the design from the N6 Discovery kit as much as possible. However, in that design the input and output capacitance for the switching regulator (U2 - TPS62088YFP) is more than four times as large as what Texas Instruments recommends for this IC (4u7F input capacitor, 2x10uF or 1x22uF output capacitance). I'd love to leave out a few of these large capacitors but before I do it would be great to understand why the designers of the Discovery kit did it this way, maybe they found during testing that TI's recommendation was not enough? Is it safe to leave out, say, halve of these capacitors?
Thanks a lot for all your help!
Kind regards, Michael