Skip to main content
Visitor II
July 5, 2025
Question

STM32N6: simultaneous MIPI interface possible for 5 MP & optical light engine?

  • July 5, 2025
  • 1 reply
  • 306 views

Hello All,

I have a camera of 5 MP and optical light engine with display of 1280 x 720 pixels.

Can I run both the peripherals on MIPI interface simultaneously such that the camera content is input/feed is input to optical light engine having display of 1280 x 720 pixels. I am using STM32N647A0. Do we have a running example on STM32N6. I have the N6-DK board. Please suggest and recommend.

 

Best Regards,

Sakshi 

 

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    July 18, 2025

    Hello @sakshi;

     

    Can I run both the peripherals on MIPI interface simultaneously

    Which interface do you want to use DCMIPP?

    I recommend you to referring to DCMIPP examples STM32CubeN6/Projects/STM32N6570-DK/Applications/DCMIPP at main · STMicroelectronics/STM32CubeN6 · GitHub may help you starting with camera.

    I hope this help you.

     

    Thank you.

    Kaouthar