STM32N6570-DK XSPI flash incorrect data
Hello,
I use an external flash in memory mapping mode and I have a strange problem. The application is executed from the internal RAM, while the checksum is calculated on the data from the external flash (simple summing of successive bytes in a loop). Interestingly, sometimes I get an incorrect result, i.e. the sum is a bit smaller, e.g. instead of 3233257 it is 3233225 as if one byte had not been counted. Interestingly, later the program jumps to the application that is executed from the external flash and it works normally (does not crash). I tried to turn off D-Cache but it does not help. Since the program from the flash executes correctly, I assume that it is not a problem with the memory configuration. What could it be?
EDIT:
BR
Artur