Skip to main content
Visitor II
October 30, 2025
Solved

STM32N6xxx SMPS internal , external

  • October 30, 2025
  • 1 reply
  • 143 views

Hi Everybody

1) There are some technical o specific reasons, that I was not able to find in the various documentations, to use external SMPS for VDDCORE insted of the internal one ?
2) Working on NUCLEO-N675X0-Q, to configure various bridge for internal SMPS, documentation report to remove R103.
But if this, VDDA1V8 is missing and board doesn't work.
I remove and install all bridge as reported in the documentation (UM3417) , just I left R103 ON, only in this way the board work.
Regards
Danilo

 





    This topic has been closed for replies.
    Best answer by TDK

    Details are in here:

    Getting started with hardware development for STM32N6 MCUs - Application note

    Specifically:

    TDK_0-1761827465827.png

    Make note of the timing restrictions between VDD/VDDCORE mentioned in there.

    1 reply

    TDKAnswer
    Super User
    October 30, 2025

    Details are in here:

    Getting started with hardware development for STM32N6 MCUs - Application note

    Specifically:

    TDK_0-1761827465827.png

    Make note of the timing restrictions between VDD/VDDCORE mentioned in there.