Skip to main content
Visitor II
December 20, 2025
Question

STM32U0: Will the LSESYSEN bit of RTC domain control register (RCC_BDCR) reset upon power-on reset?

  • December 20, 2025
  • 2 replies
  • 77 views

Greetings!

I have the following system:

  • STM32U073CC
  • VBAT pin is connected to a super-cap, and it's voltage was measured to be above the required minimum.

During system reset (NRST) it behaves according to my expectations, the RCC_BDCR remains unchanged, but if it is disconnected from Vcc, then upon connecting it back, the LSESYSEN bit is set to 0. This seems reasonable, and is generally not a issue to me, but the reference manual claims that this shouldn't happen? (Everything else works perfectly.)

Sha0S_0-1766270175993.png

Am I missing something obvious here?
Couldn't find any other mention of the bits behaviour.

    This topic has been closed for replies.

    2 replies

    Sha0SAuthor
    Visitor II
    December 20, 2025

    Tested it with a STM32U83 Nucleo too, had the same behaviour.

    • Removed SB2, and powered VBAT directly from a PSU.
    • The HAL automatically enables LSESYSEN if LSE is present with HAL_RCC_OscConfig.
    • Resetting the system with NRST: bit remains '1'.
    • Power-on reset by disconnecting the USB: bit set to '0', nothing else changes. (Well: LSESYSRDY is also 0 ofc.)

    Obviously HAL_RCC_OscConfig will set it back to '1' regardless.

    Sha0SAuthor
    Visitor II
    December 21, 2025

    This behaviour is the same as stated in the STM32U5 reference manual:

    Sha0S_0-1766275520533.png