STM32U3 series wake-up from Stop 3 mode on SMPS current/charge discrepancy
The datasheets for the new STM32U3 MCUs (375/385) list wake-up from stop3 on SMPS in uA (current), whereas for LDO the docs list the same specs in charge (nAs).
Checking the U5 datasheet and the numbers are correctly listed in nAs units. However, the values for U3 are 40-60uA, so if I add 's', it will result in fairly high figures. U5 MCU figures are ~150nAs.
Please confirm that if it's 40-60uAs or 40-60nAs, or something else.
Thanks.