STM32U5 board can't connect to cubeprogrammer
Hello,
I had two STM32 boards connected to the PC, and I ran the regression.sh program from SBSFU to configure one of them. However, the second board, which also had the SBSFU application installed, was configured as well. Now, the second board cannot connect to STM32CubeProgrammer. If you press the reset button, it connects momentarily, but once you release it, the connection is lost. Any help to revive the board?

when the reset is not pressed

and when reset is pressed