STM32U5 SPI DMA in DMA_LINKEDLIST_CIRCULAR mode occurs HardFault error
Hi
I use STM32U5 SPI2 in Salve mode to only receive data,and the data-size is 16Bit. Because the rate is very fast, I use the DMA_LINKEDLIST_CIRCULAR mode combined with the DMA half-full interrupt solution.
When I used HAL_SPI_Receive_DMA() to start SPI reception, I found that I encountered a Hardfault, in the following code.

I found that the hspi->hdmarx->Init.DestDataWidth value was abnormal. Because this value is not assigned in the HAL_SPI_MspDeInit() initialization function. So I added an assignment statement by myself, handle_GPDMA1_Channel0.Init.DestDataWidth = DMA_DEST_DATAWIDTH_HALFWORD, to solve the HardFault. It seems that the DMA is working normally.
The question is, is this modification possible?