Skip to main content
Visitor II
July 21, 2025
Question

STM32U5 SPI1 in Stop Mode

  • July 21, 2025
  • 4 replies
  • 389 views

I'm using an STM32U5 processor to communicate with a sensor over SPI, and I am unable to get the SPI transfer and reception to work while putting the device into STOP 0/1. The datasheet and reference manual state that this is possible with SPI1 in STOP 0/1, but the device never wakes up and the transfer doesn't complete. I am using SPI1 and HAL_SPI_TransmitReceive_DMA, along with linked list DMA mode. I have gotten the transfer to work successfully in SLEEP, with the device waking after all transfers are complete, but it does not work when putting the device into STOP 0 or STOP 1 mode. Are there any other bits that need to be set to enable STOP mode functionality with SPI1? I am using MSIK to clock the SPI, and STOP mode is working for other parts of the application (RTC, EXTI). Thank you.

    This topic has been closed for replies.

    4 replies

    ST Employee
    July 22, 2025

    Hello @jcjunker

    Using STM32U5, the LPDMA1 can only access SRAM4 in STOP modes, so, SPI1 Tx/Rx buffers and linked list nodes should be all allocated in SRAM4, could this the issue in your case? 

    jcjunkerAuthor
    Visitor II
    July 22, 2025

    @Sarra.S According to the datasheet/reference manual, GPDMA and SRAM 1-5 should work in Stop 0/1 modes with SPI1. I am using GPDMA and non-SRAM4 SRAM. Is this incorrect information or interpretation?

    jcjunkerAuthor
    Visitor II
    July 24, 2025

    @Sarra.S Is there any more information that you can provide me for this? Thanks.

    ST Employee
    July 31, 2025

    Hi @jcjunker, sorry for the delayed answer

    yes, you're right! 

    • ADC4, DAC1, LPTIM1, LPTIM3, LPUART1, SPI3, I2C3 and ADF1 are autonomous only with LPDMA1 and SRAM4.
    • LPTIM2, USARTx (x = 1 to 6), SPI1, SPI2, I2C1, I2C2, I2C4 and MDF1 are autonomous only with GPDMA1 and SRAM1 to SRAM5.

    Is the SPI autonomous mode enabled in the RCC configuration? Also, if SPI interrupts are enabled, the device  will wake up from Stop mode.

    Could you also share a code snippet? 

     

    jcjunkerAuthor
    Visitor II
    July 31, 2025

    @Sarra Yes, I have confirmed that SPI1SMEN in RCC_APB2SMENR is set (which is set by default so I'm not changing it). Interrupts are enabled, and I'm able to get SPI to work with interrupts when not using STOP mode. Below is a code snippet. SPI1 interrupts are enabled in stm32u5xx_hal_msp.c.

    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file : main.c
     * @brief : Main program body
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2025 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    
    LPTIM_HandleTypeDef hlptim1;
    
    SPI_HandleTypeDef hspi1;
    DMA_HandleTypeDef handle_GPDMA1_Channel1;
    DMA_HandleTypeDef handle_GPDMA1_Channel0;
    
    UART_HandleTypeDef huart1;
    
    /* USER CODE BEGIN PV */
    uint8_t tx_buf[7] = {0x0F | 0x80, 0};
    uint8_t rx_buf[7] = {0};
    static volatile int done;
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_GPDMA1_Init(void);
    static void MX_LPTIM1_Init(void);
    static void MX_SPI1_Init(void);
    static void MX_USART1_UART_Init(void);
    /* USER CODE BEGIN PFP */
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
    
     /* USER CODE BEGIN 1 */
    
     /* USER CODE END 1 */
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
    
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
    
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_GPDMA1_Init();
     MX_LPTIM1_Init();
     MX_SPI1_Init();
     MX_USART1_UART_Init();
     /* USER CODE BEGIN 2 */
     HAL_SuspendTick();
    
     HAL_SPI_TransmitReceive_IT(&hspi1, tx_buf, rx_buf, 2);
    
     // __HAL_RCC_LPTIM1_CLKAM_ENABLE();
    
     // HAL_LPTIM_Counter_Start_IT(&hlptim1);
     // HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
    
     // HAL_UARTEx_EnableStopMode(&huart1);
    
     // HAL_UART_Transmit_IT(&huart1, (uint8_t *)"TEST!\r\n", 7);
    
     // HAL_SPI_Transmit_IT(&hspi1, tx_buf, 2);
    
     HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);
    
     while (done == 0)
     ;
    
     HAL_UART_Transmit(&huart1, (uint8_t *)"DONE!\r\n", 7, HAL_MAX_DELAY);
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
     /* USER CODE END WHILE */
    
     /* USER CODE BEGIN 3 */
     }
     /* USER CODE END 3 */
    }
    
    /**
     * @brief System Clock Configuration
     * @retval None
     */
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Configure the main internal regulator output voltage
     */
     if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE4) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI
     |RCC_OSCILLATORTYPE_MSI|RCC_OSCILLATORTYPE_MSIK;
     RCC_OscInitStruct.HSIState = RCC_HSI_ON;
     RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.LSIState = RCC_LSI_ON;
     RCC_OscInitStruct.MSIState = RCC_MSI_ON;
     RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_4;
     RCC_OscInitStruct.LSIDiv = RCC_LSI_DIV1;
     RCC_OscInitStruct.MSIKClockRange = RCC_MSIKRANGE_4;
     RCC_OscInitStruct.MSIKState = RCC_MSIK_ON;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
     |RCC_CLOCKTYPE_PCLK3;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
     RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
     RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief GPDMA1 Initialization Function
     * @param None
     * @retval None
     */
    static void MX_GPDMA1_Init(void)
    {
    
     /* USER CODE BEGIN GPDMA1_Init 0 */
    
     /* USER CODE END GPDMA1_Init 0 */
    
     /* Peripheral clock enable */
     __HAL_RCC_GPDMA1_CLK_ENABLE();
    
     /* GPDMA1 interrupt Init */
     HAL_NVIC_SetPriority(GPDMA1_Channel0_IRQn, 0, 0);
     HAL_NVIC_EnableIRQ(GPDMA1_Channel0_IRQn);
     HAL_NVIC_SetPriority(GPDMA1_Channel1_IRQn, 0, 0);
     HAL_NVIC_EnableIRQ(GPDMA1_Channel1_IRQn);
    
     /* USER CODE BEGIN GPDMA1_Init 1 */
    
     /* USER CODE END GPDMA1_Init 1 */
     /* USER CODE BEGIN GPDMA1_Init 2 */
    
     /* USER CODE END GPDMA1_Init 2 */
    
    }
    
    /**
     * @brief LPTIM1 Initialization Function
     * @param None
     * @retval None
     */
    static void MX_LPTIM1_Init(void)
    {
    
     /* USER CODE BEGIN LPTIM1_Init 0 */
    
     /* USER CODE END LPTIM1_Init 0 */
    
     /* USER CODE BEGIN LPTIM1_Init 1 */
    
     /* USER CODE END LPTIM1_Init 1 */
     hlptim1.Instance = LPTIM1;
     hlptim1.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC;
     hlptim1.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV32;
     hlptim1.Init.Trigger.Source = LPTIM_TRIGSOURCE_SOFTWARE;
     hlptim1.Init.Period = 3199;
     hlptim1.Init.UpdateMode = LPTIM_UPDATE_IMMEDIATE;
     hlptim1.Init.CounterSource = LPTIM_COUNTERSOURCE_INTERNAL;
     hlptim1.Init.Input1Source = LPTIM_INPUT1SOURCE_GPIO;
     hlptim1.Init.Input2Source = LPTIM_INPUT2SOURCE_GPIO;
     hlptim1.Init.RepetitionCounter = 0;
     if (HAL_LPTIM_Init(&hlptim1) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN LPTIM1_Init 2 */
    
     /* USER CODE END LPTIM1_Init 2 */
    
    }
    
    /**
     * @brief SPI1 Initialization Function
     * @param None
     * @retval None
     */
    static void MX_SPI1_Init(void)
    {
    
     /* USER CODE BEGIN SPI1_Init 0 */
    
     /* USER CODE END SPI1_Init 0 */
    
     SPI_AutonomousModeConfTypeDef HAL_SPI_AutonomousMode_Cfg_Struct = {0};
    
     /* USER CODE BEGIN SPI1_Init 1 */
    
     /* USER CODE END SPI1_Init 1 */
     /* SPI1 parameter configuration*/
     hspi1.Instance = SPI1;
     hspi1.Init.Mode = SPI_MODE_MASTER;
     hspi1.Init.Direction = SPI_DIRECTION_2LINES;
     hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
     hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;
     hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
     hspi1.Init.NSS = SPI_NSS_HARD_OUTPUT;
     hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
     hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
     hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
     hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
     hspi1.Init.CRCPolynomial = 0x7;
     hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
     hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
     hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
     hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
     hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
     hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
     hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
     hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
     hspi1.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
     hspi1.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;
     if (HAL_SPI_Init(&hspi1) != HAL_OK)
     {
     Error_Handler();
     }
     HAL_SPI_AutonomousMode_Cfg_Struct.TriggerState = SPI_AUTO_MODE_DISABLE;
     HAL_SPI_AutonomousMode_Cfg_Struct.TriggerSelection = SPI_GRP1_GPDMA_CH0_TCF_TRG;
     HAL_SPI_AutonomousMode_Cfg_Struct.TriggerPolarity = SPI_TRIG_POLARITY_RISING;
     if (HAL_SPIEx_SetConfigAutonomousMode(&hspi1, &HAL_SPI_AutonomousMode_Cfg_Struct) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN SPI1_Init 2 */
    
     /* USER CODE END SPI1_Init 2 */
    
    }
    
    /**
     * @brief USART1 Initialization Function
     * @param None
     * @retval None
     */
    static void MX_USART1_UART_Init(void)
    {
    
     /* USER CODE BEGIN USART1_Init 0 */
    
     /* USER CODE END USART1_Init 0 */
    
     /* USER CODE BEGIN USART1_Init 1 */
    
     /* USER CODE END USART1_Init 1 */
     huart1.Instance = USART1;
     huart1.Init.BaudRate = 115200;
     huart1.Init.WordLength = UART_WORDLENGTH_8B;
     huart1.Init.StopBits = UART_STOPBITS_1;
     huart1.Init.Parity = UART_PARITY_NONE;
     huart1.Init.Mode = UART_MODE_TX_RX;
     huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
     huart1.Init.OverSampling = UART_OVERSAMPLING_16;
     huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
     huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
     huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
     if (HAL_UART_Init(&huart1) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN USART1_Init 2 */
    
     /* USER CODE END USART1_Init 2 */
    
    }
    
    /**
     * @brief GPIO Initialization Function
     * @param None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
     /* USER CODE BEGIN MX_GPIO_Init_1 */
    
     /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOA_CLK_ENABLE();
     __HAL_RCC_GPIOB_CLK_ENABLE();
     __HAL_RCC_GPIOE_CLK_ENABLE();
    
     /* USER CODE BEGIN MX_GPIO_Init_2 */
    
     /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
    {
     done = 1;
    }
    
    void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
    {
     done = 1;
    }
    
    void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi)
    {
     done = 1;
    }
    /* USER CODE END 4 */
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* User can add his own implementation to report the HAL error return state */
     __disable_irq();
     while (1)
     {
     }
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @param file: pointer to the source file name
     * @param line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */
    jcjunkerAuthor
    Visitor II
    July 31, 2025

    This is the updated code using STOP mode

    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file : main.c
     * @brief : Main program body
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2025 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    
    LPTIM_HandleTypeDef hlptim1;
    
    SPI_HandleTypeDef hspi1;
    DMA_HandleTypeDef handle_GPDMA1_Channel1;
    DMA_HandleTypeDef handle_GPDMA1_Channel0;
    
    UART_HandleTypeDef huart1;
    
    /* USER CODE BEGIN PV */
    uint8_t tx_buf[7] = {0x0F | 0x80, 0};
    uint8_t rx_buf[7] = {0};
    static volatile int done;
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_GPDMA1_Init(void);
    static void MX_LPTIM1_Init(void);
    static void MX_SPI1_Init(void);
    static void MX_USART1_UART_Init(void);
    /* USER CODE BEGIN PFP */
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
    
     /* USER CODE BEGIN 1 */
    
     /* USER CODE END 1 */
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
    
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
    
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_GPDMA1_Init();
     MX_LPTIM1_Init();
     MX_SPI1_Init();
     MX_USART1_UART_Init();
     /* USER CODE BEGIN 2 */
     HAL_SuspendTick();
    
     HAL_SPI_TransmitReceive_IT(&hspi1, tx_buf, rx_buf, 2);
    
     // __HAL_RCC_LPTIM1_CLKAM_ENABLE();
    
     // HAL_LPTIM_Counter_Start_IT(&hlptim1);
     // HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
    
     // HAL_UARTEx_EnableStopMode(&huart1);
    
     // HAL_UART_Transmit_IT(&huart1, (uint8_t *)"TEST!\r\n", 7);
    
     // HAL_SPI_Transmit_IT(&hspi1, tx_buf, 2);
    
     HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);
    
     while (done == 0)
     ;
    
     HAL_UART_Transmit(&huart1, (uint8_t *)"DONE!\r\n", 7, HAL_MAX_DELAY);
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
     /* USER CODE END WHILE */
    
     /* USER CODE BEGIN 3 */
     }
     /* USER CODE END 3 */
    }
    
    /**
     * @brief System Clock Configuration
     * @retval None
     */
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Configure the main internal regulator output voltage
     */
     if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE4) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI
     |RCC_OSCILLATORTYPE_MSI|RCC_OSCILLATORTYPE_MSIK;
     RCC_OscInitStruct.HSIState = RCC_HSI_ON;
     RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.LSIState = RCC_LSI_ON;
     RCC_OscInitStruct.MSIState = RCC_MSI_ON;
     RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_4;
     RCC_OscInitStruct.LSIDiv = RCC_LSI_DIV1;
     RCC_OscInitStruct.MSIKClockRange = RCC_MSIKRANGE_4;
     RCC_OscInitStruct.MSIKState = RCC_MSIK_ON;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
     |RCC_CLOCKTYPE_PCLK3;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
     RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
     RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief GPDMA1 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPDMA1_Init(void)
    {
    
     /* USER CODE BEGIN GPDMA1_Init 0 */
    
     /* USER CODE END GPDMA1_Init 0 */
    
     /* Peripheral clock enable */
     __HAL_RCC_GPDMA1_CLK_ENABLE();
    
     /* GPDMA1 interrupt Init */
     HAL_NVIC_SetPriority(GPDMA1_Channel0_IRQn, 0, 0);
     HAL_NVIC_EnableIRQ(GPDMA1_Channel0_IRQn);
     HAL_NVIC_SetPriority(GPDMA1_Channel1_IRQn, 0, 0);
     HAL_NVIC_EnableIRQ(GPDMA1_Channel1_IRQn);
    
     /* USER CODE BEGIN GPDMA1_Init 1 */
    
     /* USER CODE END GPDMA1_Init 1 */
     /* USER CODE BEGIN GPDMA1_Init 2 */
    
     /* USER CODE END GPDMA1_Init 2 */
    
    }
    
    /**
     * @brief LPTIM1 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_LPTIM1_Init(void)
    {
    
     /* USER CODE BEGIN LPTIM1_Init 0 */
    
     /* USER CODE END LPTIM1_Init 0 */
    
     /* USER CODE BEGIN LPTIM1_Init 1 */
    
     /* USER CODE END LPTIM1_Init 1 */
     hlptim1.Instance = LPTIM1;
     hlptim1.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC;
     hlptim1.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV32;
     hlptim1.Init.Trigger.Source = LPTIM_TRIGSOURCE_SOFTWARE;
     hlptim1.Init.Period = 3199;
     hlptim1.Init.UpdateMode = LPTIM_UPDATE_IMMEDIATE;
     hlptim1.Init.CounterSource = LPTIM_COUNTERSOURCE_INTERNAL;
     hlptim1.Init.Input1Source = LPTIM_INPUT1SOURCE_GPIO;
     hlptim1.Init.Input2Source = LPTIM_INPUT2SOURCE_GPIO;
     hlptim1.Init.RepetitionCounter = 0;
     if (HAL_LPTIM_Init(&hlptim1) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN LPTIM1_Init 2 */
    
     /* USER CODE END LPTIM1_Init 2 */
    
    }
    
    /**
     * @brief SPI1 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_SPI1_Init(void)
    {
    
     /* USER CODE BEGIN SPI1_Init 0 */
    
     /* USER CODE END SPI1_Init 0 */
    
     SPI_AutonomousModeConfTypeDef HAL_SPI_AutonomousMode_Cfg_Struct = {0};
    
     /* USER CODE BEGIN SPI1_Init 1 */
    
     /* USER CODE END SPI1_Init 1 */
     /* SPI1 parameter configuration*/
     hspi1.Instance = SPI1;
     hspi1.Init.Mode = SPI_MODE_MASTER;
     hspi1.Init.Direction = SPI_DIRECTION_2LINES;
     hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
     hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;
     hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
     hspi1.Init.NSS = SPI_NSS_HARD_OUTPUT;
     hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
     hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
     hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
     hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
     hspi1.Init.CRCPolynomial = 0x7;
     hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
     hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
     hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
     hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
     hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
     hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
     hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
     hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
     hspi1.Init.ReadyMasterManagement = SPI_RDY_MASTER_MANAGEMENT_INTERNALLY;
     hspi1.Init.ReadyPolarity = SPI_RDY_POLARITY_HIGH;
     if (HAL_SPI_Init(&hspi1) != HAL_OK)
     {
     Error_Handler();
     }
     HAL_SPI_AutonomousMode_Cfg_Struct.TriggerState = SPI_AUTO_MODE_DISABLE;
     HAL_SPI_AutonomousMode_Cfg_Struct.TriggerSelection = SPI_GRP1_GPDMA_CH0_TCF_TRG;
     HAL_SPI_AutonomousMode_Cfg_Struct.TriggerPolarity = SPI_TRIG_POLARITY_RISING;
     if (HAL_SPIEx_SetConfigAutonomousMode(&hspi1, &HAL_SPI_AutonomousMode_Cfg_Struct) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN SPI1_Init 2 */
    
     /* USER CODE END SPI1_Init 2 */
    
    }
    
    /**
     * @brief USART1 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_USART1_UART_Init(void)
    {
    
     /* USER CODE BEGIN USART1_Init 0 */
    
     /* USER CODE END USART1_Init 0 */
    
     /* USER CODE BEGIN USART1_Init 1 */
    
     /* USER CODE END USART1_Init 1 */
     huart1.Instance = USART1;
     huart1.Init.BaudRate = 115200;
     huart1.Init.WordLength = UART_WORDLENGTH_8B;
     huart1.Init.StopBits = UART_STOPBITS_1;
     huart1.Init.Parity = UART_PARITY_NONE;
     huart1.Init.Mode = UART_MODE_TX_RX;
     huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
     huart1.Init.OverSampling = UART_OVERSAMPLING_16;
     huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
     huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
     huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
     if (HAL_UART_Init(&huart1) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN USART1_Init 2 */
    
     /* USER CODE END USART1_Init 2 */
    
    }
    
    /**
     * @brief GPIO Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
     /* USER CODE BEGIN MX_GPIO_Init_1 */
    
     /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOA_CLK_ENABLE();
     __HAL_RCC_GPIOB_CLK_ENABLE();
     __HAL_RCC_GPIOE_CLK_ENABLE();
    
     /* USER CODE BEGIN MX_GPIO_Init_2 */
    
     /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
    {
     done = 1;
    }
    
    void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
    {
     done = 1;
    }
    
    void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi)
    {
     done = 1;
    }
    /* USER CODE END 4 */
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* User can add his own implementation to report the HAL error return state */
     __disable_irq();
     while (1)
     {
     }
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @PAram file: pointer to the source file name
     * @PAram line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */