STM32U5 tinyusb host mode driver help
Hey!
I'm trying to create a driver for the STM32U545 for TinyUSB . Currently, theres a driver existing for device mode, and theres driver for the boards using synopsys and not usb_fsdev. I have followed the reference manual, and gotten so far:
hcd_stm32_fsdev.c (the driver itself)
stm32_helpers.h (helper function for different accesses)
It detects the device, and starts sending some data, but then it just stops. Here's full stack trace:
[13:54:09.609] Welcome to our controller!
[13:54:13.617] [0:] USBH Device Attach
[13:54:13.771] Device unplugged while debouncing
[13:54:13.930] [0:] USBH Device Attach
[13:54:14.133] Full Speed
[13:54:14.146] [0:0] Open EP0 with Size = 8
[13:54:14.154] Get 8 byte of Device Descriptor
[13:54:14.162] [0:0] Get Descriptor: 80 06 00 01 00 00 08 00
[13:54:14.176] [:0] on EP 00 with 1 bytes: OK
[13:54:14.185] [:0] on EP 80 with 1 bytes: OK
[13:54:14.193] [0:0] Control data:
[13:54:14.198] 0000: 00 |.|
[13:54:14.215] [:0] on EP 00 with 1 bytes: OK
[13:54:14.224] Set Address = 1
[13:54:14.228] [0:0] Set Address: 00 05 01 00 00 00 00 00
[13:54:14.242] [:0] on EP 00 with 1 bytes: OK
[13:54:14.251] [:0] on EP 80 with 1 bytes: OK
[13:54:14.260] [0:1] Open EP0 with Size = 0
[13:54:14.268] Get Device Descriptor
[13:54:14.274] [0:1] Get Descriptor: 80 06 00 01 00 00 12 00
[13:54:14.288] [:1] on EP 00 with 1 bytes: OK
[13:54:14.297] [:1] on EP 80 with 1 bytes: OK
[13:54:14.305] [0:1] Control data:
[13:54:14.310] 0000: 00 |.|
[13:54:14.327] [:1] on EP 00 with 1 bytes: OK
[13:54:14.336] [0:1] Get Descriptor: 80 06 00 03 00 00 02 00
[13:54:14.350] [:1] on EP 00 with 1 bytes: OK
[13:54:14.359] [:1] on EP 80 with 1 bytes: OK
[13:54:14.367] [0:1] Control data:
[13:54:14.372] 0000: 00 |.|
[13:54:14.389] [:1] on EP 00 with 1 bytes: OK
[13:54:14.398] [0:1] Get Descriptor: 80 06 00 03 00 00 00 00
[13:54:14.412] [:1] on EP 00 with 1 bytes: OK
[13:54:14.421] [:1] on EP 00 with 1 bytes: OK
[13:54:14.430] Get Configuration[0] Descriptor (9 bytes)
[13:54:14.440] [0:1] Get Descriptor: 80 06 00 02 00 00 09 00
[13:54:14.454] [:1] on EP 00 with 1 bytes: OK
[13:54:14.463] [:1] on EP 80 with 1 bytes: OK
[13:54:14.471] [0:1] Control data:
[13:54:14.477] 0000: 00 |.|
[13:54:14.493] [:1] on EP 00 with 1 bytes: OK
[13:54:14.502] Get Configuration[0] Descriptor
[13:54:14.510] [0:1] Get Descriptor: 80 06 00 02 00 00 00 00
[13:54:14.524] [:1] on EP 00 with 1 bytes: OK
[13:54:14.533] [:1] on EP 00 with 1 bytes: OK
[13:54:14.542] Set Configuration = 1
[13:54:14.547] [0:1] Set Configuration: 00 09 01 00 00 00 00 00
[13:54:14.562] [:1] on EP 00 with 1 bytes: OK
[13:54:14.571] [:1] on EP 80 with 1 bytes: OK
[13:54:14.579] [1] Aborted transfer on EP 01
[13:54:14.587] [1] Aborted transfer on EP 81
[13:54:14.595] [1] Aborted transfer on EP 02
[13:54:14.602] [1] Aborted transfer on EP 82
[13:54:14.610] [1] Aborted transfer on EP 03
[13:54:14.618] [1] Aborted transfer on EP 83
[13:54:14.626] [1] Aborted transfer on EP 04
[13:54:14.633] [1] Aborted transfer on EP 84
[13:54:14.641] [1] Aborted transfer on EP 05
[13:54:14.649] [1] Aborted transfer on EP 85
[13:54:14.656] [1] Aborted transfer on EP 06
[13:54:14.664] [1] Aborted transfer on EP 86
[13:54:14.672] [1] Aborted transfer on EP 07
[13:54:14.680] [1] Aborted transfer on EP 87
[13:54:14.687] [1] Aborted transfer on EP 08
[13:54:14.695] [1] Aborted transfer on EP 88
[13:54:14.703] [1] Aborted transfer on EP 09
[13:54:14.711] [1] Aborted transfer on EP 89
[13:54:14.718] [1] Aborted transfer on EP 0A
[13:54:14.726] [1] Aborted transfer on EP 8A
[13:54:14.734] [1] Aborted transfer on EP 0B
[13:54:14.742] [1] Aborted transfer on EP 8B
[13:54:14.749] [1] Aborted transfer on EP 0C
[13:54:14.757] [1] Aborted transfer on EP 8C
[13:54:14.765] [1] Aborted transfer on EP 0D
[13:54:14.772] [1] Aborted transfer on EP 8D
[13:54:14.780] [1] Aborted transfer on EP 0E
[13:54:14.788] [1] Aborted transfer on EP 8E
[13:54:14.796] [1] Aborted transfer on EP 0F
[13:54:14.803] [1] Aborted transfer on EP 8F
[13:54:14.812] Device configured
[13:54:14.816] Parsing Configuration descriptor (wTotalLength = 0)
[13:54:23.786] [0:0:0] USBH DEVICE REMOVED
[13:54:23.793] [0:0:0] unplugged address = 1
I'm looking for any help in making it work, however I dont really know how to troubleshoot more. Every tips is appreciated :)