STM32U545RE USART3 issue
Hello
I am using STM32U545RE (LQFP64 package) for my project as master controller. I am using the following pins for USART3 along with a transceiver chip ADM3061E

and an additional GPIO output configured to act as the Enable.
USART3_RX:PC5
USART3_TX:PC4
Enable:PB1
But on transmitting the data I am not getting any data on the output A,B pns(as in diagram).
But the same works with STM32L496RE uC, may I know what is the cause of this problem here?
On referring to the STM32U545xx Errata sheet, we got to know that the device that I use also has Z marking.
Is there a workaround available if the above problem is because of the untrimmed uC samples?
Regards
Roshan Anand