Question
STM32U575 ADC1 AWD1 Interrupt handler abnormal
The awd1 interrupt is enabled. The flags of awd1 and EOS are set before entering the ADC1_IRQHandler. If the flag of awd1 is handled first in the ADC1_IRQHandler, the flag of EOS will not be handled. If the flag of EOS is handled first in the ADC1_IRQHandler, the flag of awd1 will not be handled. It seems that when I clear one flag first, the others disappear.
void ADC1_IRQHandler(void)
{
if((ADC1->ISR & ADC_ISR_AWD1_BIT) != 0)
{
ADC1->ISR |= ADC_ISR_AWD1_BIT;
ADC1->LTR1 = 0x00000000u;
ADC1->HTR1 = 0x00003FFFu;
}
if((ADC1->ISR & ADC_ISR_EOS_BIT) != 0) // Always be false
{
/* Clear flag ADC group regular end of sequence conversions. */
ADC1->ISR |= ADC_ISR_EOS_BIT;
}
}
void ADC1_IRQHandler(void)
{
if((ADC1->ISR & ADC_ISR_EOS_BIT) != 0)
{
/* Clear flag ADC group regular end of sequence conversions. */
ADC1->ISR |= ADC_ISR_EOS_BIT;
}
if((ADC1->ISR & ADC_ISR_AWD1_BIT) != 0) // Always be false
{
ADC1->ISR |= ADC_ISR_AWD1_BIT;
ADC1->LTR1 = 0x00000000u;
ADC1->HTR1 = 0x00003FFFu;
}
}