Skip to main content
Visitor II
May 29, 2023
Question

STM32U575 Analog Watchdog with Oversampling on ADC1. Need clarification of the reference manual

  • May 29, 2023
  • 1 reply
  • 1510 views

Hi,

One of our project is using the STM32U575 and we use the ADCs analog watchdog feature of the CPU. At the beginning of the project, we did not used the ADC oversampling, but for stability and reliability purpose, we have turned on the ADC oversampling on ADCs.

Reading the RM, the ADCs analog watchdog thresholds need some adjustements when used in oversampling mode, but it is not clear about that, and the STM32 HAL / LL comments are not giving the same values that the RM.

1/ In the RM rev 4.0, in the note of the Table 313 (Chapter 33.4.30), it is written that the watchdog comparison is performed when the oversampling, gain and offset are complete.

2/ In RM chapter 33.4.31 (about oversampler), it is also written that the comparison is done on the oversampled accumulated value BEFORE shifting. However, the note right after (which is probably a copy paste from the same capter for ADC4) tells that the oversampler shift value will have an impact on the thresholds. Also, it tells that the comparison is done between ADC_DR and the HT/LT, but ADC_DR is the final data result AFTER shift is applied. That's the first clarification that I need

3/ In the STM32Cube HAL driver (file stm32u5xx_hal_adc.c), which I read for reference (we use the LL drivers for more flexibility and control), the HAL_ADC_AnalogWDGConfig uses as paremeter a ADC_AnalogWDGConfTypeDef structure. Looking at its definition, for the Thresholds, there's an interesting comment :

"Note: If ADC oversampling is enabled, ADC analog watchdog thresholds are impacted:  the comparison of analog watchdog thresholds is done on oversampling intermediate computation (after ratio, before shift application): intermediate register bitfield [32:7] (26 most significant bits)."

Well, it is interesting, but where does the [32:7] come from ? There's no trace anywhere else. Does it mean that the "oversampled intermediate computation" is left-aligned ? Also, 26-bit comparison with HT/LT values which are 25-bits long seems strange.

4/ After reading all the documentation probably 20 times, reading the HAL code to detect any tricks, I've not been able to find the real way to compute the threshold, so I started experimenting on the real board, with some debug access. The ADC1 is configured with 10-bit resolution, and Analog Watchdog 1 is used on a channel where a constant DC voltage is fed. Here are the results :

  • Test 1 : Oversampling set to 8x, Right shift set to 3. If I follow the RM, the threshold should simply be multiplied by 8 (oversampling ratio). I found that I need it to multiply the threshold value (expected in ADC_DR value) by 16 ( = ADC Oversampled value * 2)
  • Test 2 : Oversampling still set to 8x, Right shift set to 2. Threshold should not have to be changed because comparison is done BEFORE shifting (as per RM). I found that I need to multiply the threshold value (expected in ADC_DR value) by 16 ( = ADC Oversampled value * 4)
  • Test 3 : Oversampling still set to 8x, Right shift disabled. I found that I need to multiply the threshold value (expected in ADC_DR value) by 16 ( = ADC Oversampled value * 16)
  • Test 4 : Oversampling set to 16x. Right shift set to 3. I found that I need to multiply the threshold value (expected in ADC_DR value) by 16 ( = ADC Oversampled value * 4)

=> It seems like I need to do a left shift of the threshold by 4 to compute the threshold, but that's not what I expect when I read the RM (that's what I expect for ADC4, but nor for ADC1), however, I've not yet made the test if I use a larger right shift that the oversampling ratio (let say oversampling 8x, and right shift 4).

These results are observations on the real hardware, with a constant DC signal at the ADC input, and only playing with ADC registers directly, so there's no software related, only ADC1 CFGR2 and HT1/LT1 registers are changed.

Therefore I need some help to understand how is the ADC1 Analog Watchdog threshold computation supposed to be done. Examples are welcome to illustrate the explanation, because the RM is not very helpfull on these points (there's no description of the ADC raw value format, is it right or left aligned, how is it used when the resolution is less than the full resolution, is data right or left aligned in the accumulator, ...).

Regards, Jerome

    This topic has been closed for replies.

    1 reply

    Explorer
    October 9, 2024

    I never use bloatware HAL library, but only LL library. From LL_ADC_ConfigAnalogWDThresholds description, you can see:

     

    * @note If ADC oversampling is enabled, ADC analog watchdog thresholds are
    * impacted: the comparison of analog watchdog thresholds is done on
    * oversampling final computation (after ratio and shift application):
    * ADC data register bitfield [15:4] (12 most significant bits).
    * Examples:
    * - Oversampling ratio and shift selected to have ADC conversion data
    * on 12 bits (ratio 16 and shift 4, or ratio 32 and shift 5, ...):
    * ADC analog watchdog thresholds must be divided by 16.
    * - Oversampling ratio and shift selected to have ADC conversion data
    * on 14 bits (ratio 16 and shift 2, or ratio 32 and shift 3, ...):
    * ADC analog watchdog thresholds must be divided by 4.
    * - Oversampling ratio and shift selected to have ADC conversion data
    * on 16 bits (ratio 16 and shift none, or ratio 32 and shift 1, ...):
    * ADC analog watchdog thresholds match directly to ADC data register.

    The description is very confusing. What you need to do when using oversampling and analog watchdog at the same time:
    If you are using 12 bits ADC results, divide thresholds by 16

    If you are using 14 bits ADC results, divide thresholds by 4

    If you are using 16 bits ADC results, no need to divide

    I have tested with STM32G030, this works without issue.