STM32U575 Boot up power consumption
Hi All,
I am trying to reduce the boot up power consumption using STM32U575RIT6xQ . I using a 4-20mA power source and the boot up power is 7.6mA. After it boots up the power consumption is 3.4mA.
We are using Free RTOS. Below is the pins that are activated :
1. ADC1 3 Channels
2. GPIO 26 Pins
3. I2C2 2 pins
4. TIM 2 timers
5. UART4
6. USART3 Asynchronous
My requirement is the device should boot up and run below 3.5mA. Is there a way to reduce it in the firmware at the boot up.
I am aware that power saving mode can be implemented in the code but not sure how to reduce power at boot up. If anyone could provide any assistance it would be very helpful
Thank You in advance