Skip to main content
Visitor II
March 13, 2024
Question

STM32U575 MMC operation issue

  • March 13, 2024
  • 0 replies
  • 862 views

Hi,

I need help on MMC operations.

My project is using STM32U575 to access MMC chip (EMMC16G-IB29). It uses SDMMC1  on 4B bus (MMC 4bit wide bus). The U575 is running on 90MHz. The initialization sub is:

 

static void MX_SDMMC1_MMC_Init(void)

{

hmmc1.Instance = SDMMC1;

hmmc1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;

hmmc1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;

hmmc1.Init.BusWide = SDMMC_BUS_WIDE_4B;

hmmc1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;

hmmc1.Init.ClockDiv = 3;// less than 3 won't work

if (HAL_MMC_Init(&hmmc1) != HAL_OK)

{

Error_Handler();

}

}

 

I can perform erase, write, and read operations on this chip without issues using the HAL_MMC_WriteBlocks() and HAL_MMC_ReadBlocks() function calls. However, when I switch to using HAL_MMC_WriteBlocks_DMA() and HAL_MMC_ReadBlocks_DMA(), the program halts at SDMMC_GetCmdResp1().

Interestingly, if I insert a break-point after HAL_MMC_WriteBlocks_DMA(), then continue, the MMC operation succeeds. It seems like there might be some timing issues, although HAL_MMC_WriteBlocks_DMA() returns HAL_OK, indicating a successful operation.

 

The testing function is

 

uint8_t Test_eMMC(void)

{

uint8_t ret = HAL_OK;

 

if(Wait_MMCCARD_Ready() != HAL_OK)

{

_eMMC_Error_Handler();

}

 

if(HAL_MMC_Erase(&hmmc1, ADDRESS, ADDRESS + MMC_LOG_BUFSIZE) != HAL_OK)

{

_eMMC_Error_Handler();

}

 

if(Wait_MMCCARD_Ready() != HAL_OK)

{

_eMMC_Error_Handler();

}

/* Fill the buffer with 0, 1, 2, ... */

for (uint16_t i = 0; i < MMC_LOG_BUFSIZE; i++)

{

MMC_Log_Buf[i] = (i & 0xff);

}

 

if(Wait_MMCCARD_Ready() != HAL_OK)

{

_eMMC_Error_Handler();

}

 

if(HAL_MMC_WriteBlocks_DMA(&hmmc1, MMC_Log_Buf, ADDRESS, MMC_LOG_BUFSIZE/MMC_SECTOR_SIZE)!= HAL_OK)

{

_eMMC_Error_Handler();

}

 

if(Wait_MMCCARD_Ready() != HAL_OK)

{

_eMMC_Error_Handler();

}

 

/* Clear buffer */

for (uint16_t i = 0; i < MMC_LOG_BUFSIZE; i++)

{

MMC_Log_Buf[i] = 0;

}

 

/* read back from MMC */

if (HAL_MMC_ReadBlocks_DMA(&hmmc1, MMC_Log_Buf, ADDRESS, MMC_LOG_BUFSIZE/MMC_SECTOR_SIZE) != HAL_OK)

{

_eMMC_Error_Handler();

}

 

return HAL_OK;

}

 

uint8_t Wait_MMCCARD_Ready(void)

{

uint32_t loop = MMC_TIMEOUT;

while(loop > 0)

{

loop--;

if(HAL_MMC_GetCardState(&hmmc1) == HAL_MMC_CARD_TRANSFER)

{

return HAL_OK;

}

}

return HAL_ERROR;

}

Did I miss something for the MMC DMA operations? Thanks.

 

Regards

HGUAN

 

 

    This topic has been closed for replies.